We have a question about TPS561201.
Please show us the waveform of load transient response under the following condition.
Vin=12V
Vout=3.3V
current : 0.1A→1.0A
We can allow the change of input voltage(12V) if Vout is 3.3V.
For example, Vin is 5V, 15V and so on.
Can you show the data?
Best regards,
Takahiro Nishizawa