This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5119: When the output of LM5119 is idle, the input power consumption is too large (0.1a 48V). What is the reason for this?

Expert 2630 points
Part Number: LM5119


When the output of LM5119 is idle, the input power consumption is too large (0.1a 48V). What is the reason for this?
We made the products according to the attached schematic diagram
48 v input
Output 8 a 42 v
When the output is 0 load, the input power consumption is 48V, 0.1a?What's the reason?