This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53622: Power Sequencing Inputs Needed

Part Number: TPS53622
Other Parts Discussed in Thread: CSD95492QVM

Hi,

I am using TPS53622A and need help for the below requirement:

We noticed power up sequencing needed for TPS53622A with Power Stage CSD95492QVM is 3.3V>>5V>>12V>>VR_EN.

Our Board we are generating 3.3V from 12V (coming from external card) only. So it seems 12V is already enabled for this situation. Please suggest any recommendation for the problem or someway we can tweak sequencing. Any power switch with enable control we can use ??

Another Query: We have our vendor board and it seems they used  5V>>3.3V>>12V>>VR_EN . Is there any impact for this sequence ??

Regards,

Vikas G.