Hi,
I performed the cycle to obtain the chem ID of my battery.I have a deviation of 8.44%.the app note SLVA 725 recommends less than 3%.
I would like to know if a deviation of 8.44% will create a large measurement errors during the life of the battery?
Does the learning cycle also helps to improve the accuracy of the gas gauge too?
Regards,
Clement
Chemistry ID selection tool, rev=2.48 Configuration used in present fit: ProcessingType=2 NumCellSeries=4 ElapsedTimeColumn=0 VoltageColumn=1 CurrentColumn=2 TemperatureColumn=3 Best chemical ID : 457 Best chemical ID max. deviation, % : 8.44 Summary of all IDs with max. DOD deviation below 15% Chem ID max DOD error, % Max R deviation, ratio 457 8.44 0.18 446 11.03 0.03 478 11.47 0.01 435 11.49 0.96 6106 11.53 0.58 462 12.05 0.79 436 12.38 0.92 425 12.45 0.54 464 12.47 0.75 450 12.97 0.73 445 13.65 0.84 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 354 bq27411-G1C: 4.35V LiCoO2 33.81 3142 bq27421-G1D: 4.4V LiCoO2 34.76 128 bq27421-G1A: 4.2V LiCoO2 3072.65 312 bq27421-G1B: 4.3V LiCoO2 4791.99 Best generic ID 354 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 33.81 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 42.06 1202 bq27621: (default) 4.2V LiCoO2 2776.45 Best generic ID 354 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3230 bq27426: (default) 4.35V LiCoO2 28.34 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 34.76 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 2776.45 Best generic ID 3230 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Warning: First OCVpoint has non-zero current I= -0.003 Please make sure you have a 2 hr relaxation period before the beginning of discharge. Warning: Last OCVpoint has non-zero current I= -0.003 Please make sure you have a 5 hr relaxation period after the end of discharge.