This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40090: how to use TPS40090 for 45A current source?

Part Number: TPS40090

Customer has the below applcation:

12V input, <= 3V output, with 45A constant  output current.

Could you help suggest how to use TPS40090 together with external current loop to deal with this? TPS40090 is a 4-Channel MultiPhase controller, but I think 2 phase is enough for this current, do you have any other better suggested part? Thank you.