This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24190: Problems that can not be charged from the PC

Part Number: BQ24190

Hi Team

My customer is facing the problem that can not be charged from the PC.

And my customer understood below 2 IC functions from the datasheet.

The conditions for entering the HIZ state are

・ USB Input source is USB Host (SDP 100mA)

・ Battery voltage VBAT> VBATGD (3.55V)

When IC enters HIZ, sleep mode close to shutdown.

Then the customer asked and requested below, Please advise,

1. When BQ24190 is in host mode, please explain the relationship between the timing when INT is set and the timing when entering HIZ.

2. Is the timing when bit is set in REG [00] 7 after HIZ state?

3. What are the timing constraints for detecting INT from Host and releasing HIZ?

4.Please send the entire state transition diagram and timing chart of BQ24190.

 

If the BQ24190 is in host mode, the HIZ state is kept even if the USB plug is removed. Is the following understanding correct?

1. Even if the USB plug is unplugged, the HIZ state keeps and INT level doesn't change (no interrupt)

2. Since the HIZ state is kept even if the AC adapter (that is, DCP) is inserted next time, INT level does not change.

Thanks

Best regards,

Shidara