We are generating 5V@ 6A from 12V input.
The same 5V is diode OR ed with another battery source to power load when TP568215 is OFF.
Currently we used 47nF as the soft-start capacitor, as per equation 3 from datasheet, soft-start time is 4.7mS.
As we have diode OR with another low voltage source , when the TPS568215 enabled to generate 5V it will see pre-biased load, How the soft-start calculations will work with pre-biased load.
2nd question is, After enable reaches its turn ON threshold(1.225V), VREG5 starts and reaches its VREG5 UVLO - there is no data time taken in datasheet(figure 21) - Any data on approximate time to reach VREG5 UVLO after Enable crossed Turn ON threshold.