This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: Differential pair impedance

Part Number: BQ79606A-Q1
Other Parts Discussed in Thread: BQ79606-Q1

Hi there!

I'm developing a PCB with a couple of BQ79606-Q1. I would like to know If there is a specific impedance I should achieve when routing the differential pair lines needed for daisy chain communication.

Also, how critical is this for the communications?

Thanks! 

  • Hello Juan,

    This is not critical for communication but we still recommend engineers to follow design criterion of differential pair.

    See more details in application note-SLUA811.

    Differential Communication
    Maintaining signal integrity while in a stacked configuration is critical to the success of this part. In order to
    maximize immunity to interfering signals there are a couple design choices that need to be made. For
    transformer based communication, be sure to select a transformer that provides isolation appropriate for
    the specific application so ignore point number 5.
    1. Keep wires and PCB traces as short as possible. Do not exceed datasheet recommendations.
    2. For any single-signal pair between two nodes (ICs), individual wires and traces should have the
    same length.
    3. Unshielded, twisted-pair wiring is required for any cable runs.
    4. Run PCB traces in parallel, on the same layer, without any other traces or planes in between. Long
    runs should avoid noisy traces and/or be stitched at intervals similar to twisted-pair wire.
    5. Use high-quality capacitors for voltage isolation between ICs and place in close physical proximity
    to each other as part of the parallel-track layout

    Andy