This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576: How to design a heat sink?

Part Number: LM2576
Other Parts Discussed in Thread: LMR14030, LMR16030

Dear All,

Please consider an adjustable version of LM2576 supplied with a 24V or 15V ( if possible ) at input and the output= 13.2V @ 3A.

The ambient temperature range: 25-60 degC

If input voltage= 24V, the dissipation power= 2.5W and for 15V is 3.9W.

Please suppose the maximum of junction temperature= 125 degC.

For example: 60 degC

24V: the junction-to-ambient thermal resistance= 26 degC/W.

15V: the junction-to-ambient thermal resistance= 16.7 degC/W.

Should I to place a copper area on the PCB to sink the heat?

How can I calculate a heat sink embedded in the PCB?

Best Regrads, Ras