This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1101 for dc/dc switching regulator

Other Parts Discussed in Thread: CC1101, TPS62840

We are looking for a high efficiency dc/dc switching power supply for a CC1101/MSP430 based sensor node operating in the 868 MHz band.

Input supply is two 3V batteries in series. Since the input is 6V, we can't use the bypass option on a DC/DC regulator.

Required output is 3V (with max current of 100 mA).

Deep sleep current consumption of the radio/micro/sensors on our node is around 2 uA. We are looking for a regulator which will increase the sleep mode current consumption by at most 2 uA.