Hi team,
I would like to know tD, tr, tf parameter (typ/min/max) in the datasheet at the following condition.
1. VIN=VON=VBIAS=3.3V, CT=470pF
2. VIN=1.8V, VON=VBIAS=3.3V, CT=470pF
Could you advise the value?
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I would like to know tD, tr, tf parameter (typ/min/max) in the datasheet at the following condition.
1. VIN=VON=VBIAS=3.3V, CT=470pF
2. VIN=1.8V, VON=VBIAS=3.3V, CT=470pF
Could you advise the value?
regards,
Hi Shinji Tsuji,
Unfortunately, we cannot provide any testing parameters for tf for CT values less than what is stated in the datasheet. Due to the quick output discharge nature of the part, there is no difference on the falling time over different CT capacitance. Similarly, as long as Von>Vih, the effect of different Von is not significant to the timing. All timing below is in us.
1. At VIN=VBIAS=3.3V, CT=470pF
Parameter | min | typ | max |
t_r | 714.59 | 779.77 | 865.29 |
t_d | 292 | 351.56 | 426.5 |
2. At VIN=1.8V, VBIAS=3.3V, CT=470pF
Parameter | min | typ | max |
t_r | 413.81 | 449.51 | 495.38 |
t_d | 264.5 | 324.75 | 404 |
Thanks you for choosing TI Power Switches in your designs.