This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it good choice for power bank?

Part Number: BQ25890
Other Parts Discussed in Thread: BQ25895

Tool/software: WEBENCH® Design Tools

Hi,

We are look for power bank solution. The requirements as following:

  • one of micro USB connector - for power input (ex: USB charger, adapter)
  • one of USB type A female connector - for load (ex: phone, tablet)
  • one 7000 mAh li-ion battery cell (charge current can be 2 ~ 3.5A and over voltage >4.2V or 4.3V)
  • disable the output for the delivery and shipment
  • low power dissipation

Is a bq25890 good choice?

Best Regards,

Aaron