Hi,
Recently I've made a new version of a BMS for a 10S battery based on a schematic by earlier designer. The problem that I got is that after powering the BMS all but one of the balancing MOSFETs are ON. The one that is not on is on first cell. Given that the battery has 3.73V on each cell, the voltages between VC0-VC1 and so on are just the same. From the software side all balancing is disabled. Any obvious mistakes that I made ?