This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for the recommendation for replacing ME6228

Other Parts Discussed in Thread: TPS709

Hi Team,

Customer is looking solution to replace ME6228

 

Would you please recommend the proper solution for this?

https://www.elinfor.com/pdf/ETC/ME6228-ETC.pdf

 

 

BR,

SHH

 

  • Hi SHH,

    I would strongly recommend leveraging our TPS709 against the ME6228. Here is a quick comparison. Hope this helps!

    GPN ME6228 TPS709
    AEC Q100 NO NO
    Output Options Fixed Output Fixed Output
    Iout (Max) (A) 0.15 0.15
    Vin (Max) (V) 30 30
    Vin (Min) (V) 2.5 2.7
    Vout (Max) (V) 5 6
    Vout (Min) (V) 1.5 1.2
    Fixed Output Options (V) 2.5, 2.8, 3, 3.3, 3.6, 5 1.2, 1.35, 1.5, 1.6, 1.8, 1.9, 2.5, 2.7, 2.8, 3, 3.3, 3.6, 3.8, 3.9, 5, 6
    Enable NO YES
    Power Good NO NO
    Output Capacitor Type Ceramic Ceramic
    PSRR @ 100KHz (dB) - 26
    Noise (uVrms) - 190
    Accuracy (%) 2 2
    Vdo (Typ) (mV) 450 300
    Iq (Typ) (mA) 0.0015 0.001
    Thermal Resistance θJA (°C/W) 130 73
    Min Package Area (mm2) 4.64 4
    Package Type SOT-23, TO-92, SOT-89 SOT-23, WSON