Other Parts Discussed in Thread: LM5170
Hi Tiers
My project details as below:
input: 12V-32V, output: 48V 30A
does the LM5176 can support this project? Suggestions are welcome from you, thx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jack,
Thank you for reaching out. The answer is no because this is 1.5kW and the LM5176 driver cannot drive the FETs required to processing 1.5W. Each LM5176 can support up to 300W, and you would need 6 phases.
We do have a device to support such high power: the LM5170. Each Lm5170 is two phase. You can do this in three or 4 phases. Please order 2 LM5170 EVM, and configure them in 3 or 4 phases boost mode, and you can do a quick evaluation.
Thanks,
Youhao Xi, Applications Engineering