This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116-12EVAL: IC temperature issue under light loading

Part Number: LM5116-12EVAL
Other Parts Discussed in Thread: LM5116

hi Team,

customer using LM5116 for BBU solution.

test condition Vin 60V output 12V, current = 0.1A

on customer's pcba the LM5116 IC will go up to 70 degC.

but on LM5116 EVM will only go up to 45 degC. 

is there IC Tj plot graph for the EVM that's available to check the Tj value.

Thanks