Other Parts Discussed in Thread: UCC27511A
Dear ALL
Pls help me customer is need to know feature differential input of UCC27538 .
Thank you so much & Bestregard
Prarinya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Prarinya,
Thanks for your help promoting our drivers, my name is Mamadou Diallo from the High Power Drivers' team.
I am not sure I understand your question, are you asking whether the input of UCC27538 are differential inputs or what specifically about the inputs of UCC27538 that customer is inquiring about?
Can you please clarify?
Regards,
-Mamadou
Hi Mamadoa
Thank you for your help , Customer it used driver 1EDN7550B this part is true differential input Then customer is asking the equivalent the current part , customer is asking about UCC27538 have true differential input feature yes or not ?
Pls help to suggestion to me.
If possible Pls send private e mail to me .
Thank you so much & Bestregard
Prarinya
Hi Mamadou
Pls help to check differential input feature this part too UCC27511A ,customer is need to know of this feature .
Thank you so much & Bestregard
Prarinya
Hi Prarinya,
UCC27511A's input pins are both referenced to GND pin. This driver does NOT have a differential input type where the input pins are referenced to each other. Assuming VDD> UVLO, when an high input command is applied to the non-inverting IN+, the driver's output will go high when IN+ is at 2.2V(typ.) with respect to GND pin while IN- is also tied to GND. Similarly when in inverting configuration, the output will go High when IN- receives a signal <1.2V(typ.) with respect to GND pin while IN+ is tied to VDD.
Please let us know if this addresses your inquiry by clicking the green button or further post on this thread.
Thanks.
Regards,
-Mamadou