This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61160A: ESD Test failed

Part Number: TPS61160A


Hi TI,

Need your strong support here.

My customer are performing ESD test on the TPS61160ADRVR. The test will be performed from voltage +-2kV up to +-15kV. It is reported that during the -5kV test, TPS61160ADRVR has shutdown and not able to auto recover. However, when they reboot the power source manually only(Unplug and plug the AC) then the LED driver is able to boot and working again. 

May I know what is possible failure for this ESD test? Can TPS61160ADRVR theoretically able to pass the 5kV test?

BR,

Zhao Yang