This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS723-Q1: thermal dissipation in the Layout

Part Number: TPS723-Q1

Hello team,

I am designing a supply with TPS72301-Q1. It has 200mA output. I assume thermal dissipation needs to be taken care by increased area of PCB copper. To which pin I should connect those copper, GND, IN or OUT? Usually LDO has a thermal PAD for heat dissipation but it is existing in this LDO. Please advise. Thanks.

Jessica

  • Hi Jessica, 

    Normally LDO datasheet contains a recommended layout example. For this device, as you can see here. You can have different copper to connect IN, OUT and GND as shown.

    Regards, 
    Jason Song

  • Hi Jason,

    Got it. Thank you very much for your kindly support. 

    Best regards

    Jessica

  • Hi Jason,

    Another short question about which pin is the main pin used for heat dissipation? Is Ground pin? Since i want to have copper in the back side of the board and not sure which pin's copper should i give the biggest area. Could you please kindly help to confirm that again? Thank you very much for your kindly support.

    Best regards

    Jessica

  • Hi Jessica, 

    For a package that does not have thermal pads, heat can be dissipated from all pins and this is the reason to maximize the copper areas each pin has access to. People normally have ground copper with the biggest area. 

    We have an application note on thermals and it has intensive coverage on the thermal performances using different layouts. Please use this one as your reference.

    Regards, 

    Jason Song