This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: Output current capability of EVM

Part Number: TPS61169

Hi Team,

My customer wants to know how much output current capability TPS61169 EVM has. They want to check if following setup is acceptable on EVM or not
Does it work well on default setting? Or Do they need to change some components to try that?

[Setup]

Vin : 5V
Vout : 20V
Iout : 100mA

Any additional advices will be appreciated.

Regards,

Takashi Onawa