This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600: accuracy of setting the minimum switching frequency

Part Number: UCC25600

Dear Team,

the "Features" describe a +/-4% accuracy for setting the minimum switching frequency. Under "Electrical Characteristics" one can find the Kico (switching frequency gain / I (RT) ) with a typical of 80Hz/uA but a min / max of 60Hz/uA / 100Hz/uA. this deviation is much larger than +/-4%.

Practical tests over several production lots confirm values in the range of 77Hz/uA and so the +/-4% spec.

My question is: Do we really have to expect the huge deviation which would result out of the Kico for setting the setting the minimum switching frequency? What is the explanation of the discrepancy between the +/-4% spec and the Kico rating? 

Thanks Lutz

  • It depends on the temperature range. The Feature says  so please read the whole sentence to make understanding.

    Programmable Minimum Switching Frequency The UCC25600 high performance resonant mode

    With 4% Accuracy (3% accuracy at controller is designed for dc-to-dc applications

    temperature range: -20°C to 105°C)

     

    Kico (switching frequency gain / I (RT) ) with a typical of 80Hz/uA but a min / max of 60Hz/uA / 100Hz/uA. If you read the table carefully, that is with temperature -40C to 125C.

    So your expectation should be made in accordance to temperature in your application.

  • Hello,

    I agree with the statement of the features (in brackets) mentioning +/-3% accuracy for the temperature range -20°C to 105°C.

    I also agree with the statement that Kico with (min 60Hz/uA) < (typ 80Hz/uA) < (max 100Hz/uA) is speced over full temp -40°C to 125°C.

    So in what temperature range are the +/-4% valid then?

    many thanks

    Lutz

  • In range of -40 to 125C. If you look at the table on page 3, you will see Fsw(min) min to typ 40.04 to 41.7 kHz to show -3.98%, and max to typ 43.36 to 41.7kHz to show +3.98%. 

  • OK, I see.

    So once the frequency is set to the 41.7kHz it will stay at that frequency over full temp with +/-4%. My problem is, that setting the frequency to the typical 41.7Hz is not accurate then. For example. If I set the IRT = 600uA my typical switching frequency results in 48kHz. And the typical would remain over full temp within +/-4%. However, the set frequency may vary between 36kHz and 60kHz due to the variation of the Kico.

    Form my understanding the spec of the Kico tolerance is the initial switching frequency tolerance and the +/-4% the switching frequency temperature drift.

    So in total over full temp the part will have a +/-24% tolerance wrt. a calculated and set IRT of 600uA.

    Is this understanding correct?

    kind regards

    Lutz

  • Hi Team,

    do you have any feedback for me?

    thanks

    Lutz

  • Kico does not affect FSW(min) tolerance.

    When FSW(min) is reached, it is in the range of 40.04kHz to 43.36kHz, in -40C to 125C.

    How much current is needed from RT to reach FSW(min) can vary 20% (Kico) but FSW(min) variation is +/-4% after it is reached.

  • OK, understood.

    so those are two different things. One is the accuracy of Fsw min ( once reached) and the other is how accuret one can set the switching frequency.

    thanks

    Lutz