Other Parts Discussed in Thread: LM5176
Hi Team,
How to choose LM5175 buck-boost MOSFET,E.g Vin:9~36V Vo:12V/10A
How to choose MOSFET QH1 QL1 Vds 60V or 40V or other ???
How about choose Vds at QH2 QL2??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tiffany,
Thank you for posting. I would strongly recommend LM5176 instead of LM5175.
To choose the MOSFETs, you need to calculate the power dissipations. Plug in the MOSFET parameters into the design calculator (link given below), you can get the conduction and switching losses. The key consideration is to minimize the overall losses.
For voltage rating, the buck leg FETs should be rated higher than the max input voltage, and the boost leg FETs rated higher than the output voltage. A good practice is to choose the FETs having at least 10%~20% voltage margin.
http://www.ti.com/lit/zip/snvc180
http://www.ti.com/lit/zip/snvc208
Thanks,
Youhao Xi, Applications Engineering