This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63030: Inductor size reduction

Part Number: TPS63030


Hi Team,

Would you advise the smaller size recommend inductor than described in the datasheet which

are all 3 mm x 3mm size.

Conditions are : Vin =3V to 4.35V, Vout=5V, Iout=500mA, OSC=default(2400KHz)

Any advice should be highly appreciated.

Thanks

Best regards,

Shidara