Hello,
We are using ULN2003A to driving relay for touch electrical switches. We got many issues while in production testing as well as site issue after some time. Most common issues in ULN 7th , 6th pin output get shorted with either COM pin or GND pin of ULN. as mentioned in datasheet each channel can drive upto 500mA still it got damage. Single relay required only 37.5mA current. ULN input given by MCU which is work on 5VDC. Relay are 12VDC.
Kindly suggest us some protection to minize this isse.
Also what if we use TBD62003AFWG? What is main difference between this? Which is better to use?