Hi,
Suggest a replacement for the BQ24005 so as to overcome the following problems with the existing IC:
- Higher charge current not supported
- Heating issue at higher charge current (I am using 1A charge current and charging voltage of 9V for 12Ah - 2S5P Li ion battery)
I need charge current of 2A and as the charger needs to interface with a host controller, it should indicate faults such as precharge timer fault, fast charge timer fault, temperature faults, charge status etc.
Thanks in advance
Regards,
Parthan