Other Parts Discussed in Thread: UCC28951
Dear sir,
I want to design 24V 62A (1500W) SMPS with 3- phase ip 350VAC to 500Vac without PFC (voltage MODE with overcurrent limit).
I am confused to decide topology for the following two option.
1) simple full-bridge topology with SG3525 ic
2) PSFB topology with UCC28950 ic.
please suggest UCC28950 is suitable for my application? I have 12V aux power supply for IC located on secondary.
I have good experience with 3525 ic and i can design power supply faster then UCC28950.
Kindly suggest SR controller if I am going for SG3525.
Also, support for excel design tools if I am going for UCC28950 in that I don't have any experience.