This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ting,
Thank you for your question. I work on the applications team in the high power drivers group.
The average bootstrap diode current will be much less than IDBoot(peak)/2. The peak bootstrap current occurs at start-up, during the initial charging of the bootstrap capacitor. Once the bootstrap node is charged up to its peak level, only a small amount of current will be needed to top it off every cycle. The average bootstrap current will drop to the approximate average current required to switch the high-side FET on and off every cycle along with the quiescent current of the driver.
You can calculate the average current using the below equation:
Iboot(avg, steadystate) = Qg * Fsw + IDDq
Where:
Qg = total gate charge
Fsw = switching frequency
IDDq = gate driver quiescent current at your selected switching frequency
For example: If driving a FET with 100nC gate charge @ 100kHz.
Iboot(avg, steadystate) = 100nC * 100 kHz + 2mA = 10mA
If this answered your question, could you please press the green button? If not feel, free to ask more questions.
Thanks and best regards,
John
All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).