This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM2596: Is it possible to increase current by using a buck converter?

Part Number: LM2596

Tool/software: WEBENCH® Design Tools

Hi Team.

I'm designing a circuit for increasing current. I have at the input 20V 500mA  but  I want something like 5V 1A or more than 1A in the outup. I've try using webench in order to get a design but Webench doesn't allow me to control the current at the input, only the voltage can be control. So my first question is if it's possible tu use a buck convertir to get the result I want? The second is how can I simulate it and control the current valor at the input.

Thanks.