This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31707: Hotswap application

Part Number: LMZ31707


Hi,

I am using the LMZ31707 to power pluggbale QSFP+ modules in the hotswap environment, How can I prevent the controller from blowing up in case a bad module is plugged in?

Thanks,

SB

  • Hi Tan,

    Perhaps an efuse with an aluminum electrolytic would help. In the case where you are hotplugging/hotswap there may be voltage transient on the input power path that can cause voltage spikes on the VIN pin. The aluminum electrolytic should help dampen the input line by keep the input voltage stable. However this is not a complete protection solution.

    It may be more appropriate to post a question to the ESD/TVS protection group on this E2E forum for more information on their device which is commonly used in hotswap environments.

    Regards,

    Jimmy

  • Hi Jimmy,

    Thanks for your reply.

    BTW, I can't find the ESD/TVS forum group under the FORUMS tab.

    Thanks,

    SB