Other Parts Discussed in Thread: TIDA-010015
Hi,
Our design is based on TI reference TIDA-010015.
In the PFC Boost section, the mosfet Q12 is getting damaged when supply is switched off at heavy loads (say 20A) at DC inputs. This is due to the overshoot due to ringing at the switching node as shown in the image. The mosfet is rated at 650V whereas the shoot goes up to 730V.
Please suggest a suitable snubber circuitry for the above application and the corresponding calculation and tuning process.