Other Parts Discussed in Thread: UCC21732, UCC21710
Hi,
I would like to use an external shunt resistor for sensing the current of my FET, and the datasheet in par. 3. mentions, that this IC supports shunt current sensing. But going through the details, in par. 8.3.7. desaturation protection is mentioned only (also in par. 9.2). So please clarify the connection of the shunt resistor, and the threshold for this protection method, because as I understood the DESAT pin cannot be used for this purpose (9V threshold).
Thanks in advance
Krisztián Somorai