Part Number: TPS62742
Other Parts Discussed in Thread: TPS62840, TPS7A02
Good day,
I am using TPS62742 in a battery-operated circuit.
Given that its maximum output current is 400 mA, I am assuming I would be able to withdraw 200 mA at 3.3V with an input voltage of 3.65V using a D-cell M class battery.
However, a similar post tends to reject such an assumption.
Could you please provide further insight?
Should I keep using TPS62742 or should I change the supply? If yes which part?
Thanks