This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
I have a BMS with BQ77915. I used your bq77915 eva board schematic.
But only I changed Rsense value and OCDP resistor value. New values are Rsense=2.5 miliohm 3Watt and Rocdp=1 M ohm.
Actually my BMS is working normally. But when Load current increase, DSG voltage and CHG voltage of BQ77915 are equal zero volt. For example load current=0.6 ampere there is no problem.
But when load current=0.7 ampere Vdsg and Vchg are equal 0 volts. Namely my BMS is not working when load current and charge current greater than 0.69 ampere. I check all but I did not any problem in my BMS.
Can you help me?
Thanks.
Alph.
Hi Alph,
If both of the FETs are turning off, then you are having either a current fault or a temperature fault during discharge. In table 5 of our datasheet, we summarize the faults and the state of the FETs in that fault. You can use this table as a checklist to make sure none of these faults are occurring. Use the fault trigger conditions as a guide and measure the voltages of the respective pins. Hopefully, you will be able to narrow down the problem from this.
Hi Shawn,
Thank you for your repply. But I did not the current problem still. My circuit is 5S.
I looked at the table 5. I did not obtain conditions of this table. Vsrp-Vsrn value is normal in beginning at the load test. But after 20-30 second Vsrp-Vsrn value is going down. Then this is zero milivolt.
I checked all of circuits and Mosfets. I did not find any problem.
I used 15 mili ohm and 7 mili ohm an 4 mili ohm and 2,5 mili ohm as RSENSE.
Today I made a new card. But I did not get a good result unfortunately. May my BQ77915 be replica?
Is there another way out in your opinion?
Regards
Alph
Hi Shawn,
My BMS card was 5S.
I looked at table 5 but I did not solve my current problem. My bms card is not working good under the load for discharging.
I tried different Rsense value and I checked all circuit and especially Mosfets circuit but I did not find any problem on my card.
I measured Vsrp-Vsrn values. For example while RSENSE=4 miliohm Vsrp-Vsrn=-33 mV and after then 25 second Vsrp-Vsrn= 0 mV and CHG-DSG are turned off.
Today I made a new bq77915 BMS card with new components. But there is no solution still.
I wonder if my BQ77915 is replica?
Do you have solution suggestion?
Regards
Alph
Hi Shawn,
I looked table 5 but I did not find any solution for my problem. My bms card is 5S and very simple.
Today I make a new BMS card with new bq77915 component but this card is not working under the load for discharge.
I there a new solution suggestion?
Thanks.
Alph
Hi Alph,
Nothing is standing out to me as being wrong on your schematic. So let's dig more into Rsns.
Do you see any change in the operation of the circuit when using those different Rsns values? Can you verify that faults occur at different currents for each of these resistors?
For choosing an Rsns value, refer to section 10.2.2.1 of the datasheet, in question 2. The Rsns value will change the current fault protection, so you want to make sure you choose the right value.
Hi Shawn,
I tried between 2 mili ohm and 50 mili ohm for Rsns resistor.
But I obtained maximum 1,19 Amper load current unfortunately.
Above 1,19 amper, CHG and DSG FET drivers (either CHG or DSG) is turned off.
I obtained maximum Vsrp-Vsrn=57 mili volts.
Sorry..
Regards
Alph.
Hi Alph,
Let's back up a little bit. For your application, what OCC and OCD do you need? From there, we will decide the correct Rsns value. Then you should be able to see the FETs turn off when those currents are obtained.
Hi Alph,
I'm not sure you have previously specified what version of the BQ7715 you have. Is it the BQ7791500? This will determine the OCC and OCD voltage thresholds.
Hi Alph,
We have 4 versions of the BQ77915. They are BQ7791500, BQ7791501, BQ7791502, and BQ7791504. The EVM uses BQ7791500. Which one of these devices are you using?
Hi Alph,
You have a BQ7791500. The OCD and OCC for this part can be found in the device configuration table in the datasheet. Once you have determined those values, walk through the design example in section 10.2.2.1 in the datasheet. Use this to determine all of the values you would like for your circuit. If you follow this outline correctly, the device should work to your specifications.
Hi Shawn,
My problem is solved. I made 2 changes:
1. I placed Rsns resistor close to IC pins.
2. I removed 100 ohm filter resistors (connected to Rsns)
1st change ok but I am not understand 2st change.
What do you say for 2st change?
Thanks and regards
Alph.
Hi Alph,
I'm glad you solved your issue! Since the sense resistor value is so small, any additional resistance between the SRP and SRN pins could cause the device to trigger at an undesired threshold. Those filter resistors probably contributed to your sense resistance and configured your device thresholds to different value.