This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A: Soft start time

Part Number: TPS61021A

Hi,

I am FAE, a distributor of TI products.
I have a question about a soft start from my customer.
In the data sheet, the typical value is 200us (output capacitor 44uF / no load).
Could you teach me Min and Max?
The value may be a reference value. There is no need to compensate.
Or is it possible to calculate the variation by calculation?

My customer performed in a 25 ℃ environment.
The result is 350us, and there are other circuits in addition to the output capacitor about 30uF as a load.
Best regards,