This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Find Isolator DC to DC solution

Other Parts Discussed in Thread: UCC2897A, TPS40091, TL431, ATL431

Please help to suggest Isolator DC48V to DC1.2V 100A solution , thanks !

  • Rogers

    At this voltage and power level we recommend one of our active clamp forward controllers like UCC2897A.  http://www.ti.com/tool/PMP8861 is an example design that is close to your design target.  Please note that at 1.2V output is below the range of a typical TL431, or even our lower voltage ATL431.  To get down to 1.2V you may need to have a DC/DC buck converter on the output, which can be done with one of our multi-phase buck controllers like TPS40091.

    Best Regards,

    Eric