Part Number: BQ24780S
What is the PMON Gain if the input power sense resistors are 5 mOhm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If you have all configurations set for 10 mOhm/10 mOhm (default settings) but instead use 5 mOhm/5 mOhm, then the PMON circuit will calculate 1/2 the true current, which will result in 1/2 the true power calculation. So, if you have the device configured for a PMON Gain of 1 uA/W, you will instead observe 0.5 uA/W.
Please note that the only recommended (and validated) values for R_AC and R_SR are 10 mOhm and 20 mOhm. Using 5 mOhm instead will have worse signal to noise ratio.
Regards,
Steve