This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: BMS battery cells proper connection

Part Number: BQ76940

Good day, I would like to ask if this is the proper orientation when I connect my 9S battery pack to the BMS board: 


I used  http://www.ti.com/lit/df/tidr773/tidr773.pdf as reference and here is my schematic file /cfs-file/__key/communityserver-discussions-components-files/196/1121.Schematic.rar I ask this because I tried to connect the battery cells this way, and couldn't power up the AFE and MCU.. after checking my board, it turns out that diode D19 has broken. I can see a hairline crack in the surface, and a connection test shows it as a short.

What could have been the reason this diode failed? I know that it was previously working, as when I didn't have my 9S battery pack yet, I can power up the AFE and MCU using a 9V source and three 220 ohm resistors to simulate the lower group of cells like this 

Thank you very much,
Robert