This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030: LMR14030 burn out

Part Number: LMR14030


Hi,

Customer use LMR14030 in 24V applicaiton, and found that it very easy burn out, the pins impedance are short to ground. 

we measured the Vin voltage waveform and not found it higher than 40V. here is customer schematic, please help review it and give comments.

Vin:24V 

Vout:5V

Iout:0.3A

LMR14030 SCH.pdf

  • Hi Betty,

    Do you mean LMR14030 was damaged or 5V load was damaged?  it burn out at what condition? 

    What's the P/N of D1? a 10uH--22uH 5A inductor is OK for this conversion, why use 2pcs 22mH inductor? normally the 22mH inductor has quite small current rating, it maybe saturated in this application and cause device damaged.

  • Hi Andy,

    LMR14030 was damaged, the P/N of D1 is SRM54ALF.

    customer also feedback that the D1 can be damaged sometimes. they made mistake about inductor value. According the eq.10, the induction vaule is about 32.9uH.

    why inductor saturation damages the device?

    thank you

  • Hi Betty,

    The saturated inductor can't limit the current peak during high side FET turn ON, too high current peak may cause EOS damage on IC and diode.