Is there a mistake in Figure 11 of the documentation for the TPS2595? Here is a screenshot of Figure 11:
The 10 mA curve is below 5.5V for all temperatures. Here is a screenshot of the specs for VOVC and VCLAMP:
Should Figure 11 be titled "VCLAMP vs Temperature"? The 10 mA curve is consistent with the typical clamp voltage, not the overvoltage clamp threshold. I hope so anyway, because the graph suggests that a 5V +/- 5% supply would potentially be clamped by this eFuse device at higher currents.
Is VOVC independent of the load current? If not, how much of a dependence is there? I don't want this device to clamp on anything less than 5.5V at any load current level.
Thanks and regards,
Greg