This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: The UCC2897A parameter is abnormal.

Part Number: UCC2897A
Other Parts Discussed in Thread: TL431,

Hi,Peter.
      I am using UCC2897A for ACF power supply. VDD power supply is 12.7v and VIN power supply is 75V.According to the internal block diagram of datasheet, the internal reference source should be 2.5v. Why are measuring pins 3, 4 and 5 all 3.2v?I set the frequency at 250KHz, but I'm actually measuring 312.5KHz.