This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1525A:Use UC1525A in the CCM Buck Converter, the high side driver is low power transformer, the low side drive is SR IC maybe.

Part Number: UC1525A

Hi TI Team

I try to use UC1525A in the CCM Buck Converter, the high side driver is a low power transformer, the low side drive is SR IC maybe.

The maximum Iout is 10A each channel.

I don't know to make sure the low power transformer operating correctly and not saturation?

Thanks