This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

low Quiescent Current 12v boost dc to dc converter regulator

Other Parts Discussed in Thread: TPS61089, LM5155, TPS61088

HI,

we are developing Li-ion battery operated device for the we need boost dc-dc converter with below specification:

1) input voltage: 3v to 5v

2) output voltage 10v@0.5A(max)

3) output voltage 12v@1A(max)

 4) With low Quiescent Current less then 1mA.

Please suggest me the any part number suitable to above specifications.

Thanks,

Ashok