Other Parts Discussed in Thread: UCC28600, , UCC28710
Hi,
We are proposing to use the UCC2871X family of PSR for our sub 70W power supplies. The input is 3 phase rectified and used in an aircraft. The voltage levels are 100V DC to 600V DC. It is similar to TIDA - 00173.
1. Is this part (family) suitable for High reliability applications.
2. We need to prove correct operation of the controller under all operating conditions and combinations. Considering adherence to the Datasheet parameters can this be established.
3. If 2 above is achievable, do you have any guidelines for testing the application.
4. Would you be willing to share the internal logic design of the controller for us to ascertain we have tested all modes, including transitional ones.
5. What is the max gate capacitance the internal driver can support using Low Vgs FET's.
6. With a Vgs of 14V, is the driver able to support SIC Mosfets.
Regards,
Murali