This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562201: max duty cycle for 5V output

Part Number: TPS562201


Does TPS562201 can support 6.6V input 5V/300mA output at 70 degree  temerature.

I use the Webench to modify the system show the input parameter coulnd't meet.

Doew AE or design team has the test data of the part output 5V/300mA min input voltage data or not, thanks.