Hello,
I would like to design +15V input to -15.5V 2.5A output with external 1MHz sync clock input with default RT set to 1MHz self switching.
In IBB application, TI provide design consideration on EN pin and PG pin also with Sync pins design consideration confirmed in this forum.
Now I am worry about others control pins like SS/TRK, RT and BIAS_SEL is there any design consideration require. Because the reference (PGND, AGND) are moving toward negative voltage after enable.
- SS/TRK connected to -14V5 output (AGND pin) with ceramic capacitor to control soft-start time. (Equation 6)
- RT connected to -14V5 output (AGND pin) with 38K3 to set internal Fsw to 1MHz. (Table 6)
- BIAS_SEL connected to -14V5 output (PGND pin) to disable internal BIAS LDO. Not sure which voltage should be provide to increase efficiency.
Best regards,
Ping