Looking for a NiCd/NiMh intelligent charger (mostly NiMh) to charge 20 cells in series and 2 such packs in parallel (2S2P).
Input 28V/I max 3A
Do we have anything to meet these needs?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Greg,
It appears that the NiMH charger will be charging at higher than the cell's 0.5C so termination by safety timer is not an option.
The only dedicated NiMH battery charger we have is the BQ2000 family. It can perform the recommended NiMH termination (dV/dt or dT/dt). With additional level shifting components, it can operate up to 28V input.
The only battery chargers with 28V input capability are the BQ24600 standalone family and BQ24703 I2C controlled charger. These are LiIon chargers and so cannot perform the recommended NiMH termination methods (dV/dt or dT/dt).
Is there a host processor and ADC that can take measurements to perform termination?
Regards,
Jeff