art Number: MC33063A
Dear all:
I'm using MC33063A with input of 10~35V and output of 5V.In the actual test, when the input VIN=24V and the load is 5V/300mA, the input current is 110mA. The conversion efficiency is 5*0.3/(24*0.11)=56.8%
But the data sheet says conversion efficiency is 83.7. Why is the result of my test 56.8%? Any Suggestions?Here is my schematic