I am using the BQ24765 with BQ20Z75.I believe it is possible to destroy the BQ2476 when the BQ20Z75 disconnects the battery at charge termination.
I am applying "How to Operate Fuel Gauge bq20z7x/8x/9x and the SMBus-Like Smart Chargers bq24747/765 Without a Host Controller" (SLUA533). My fuel gauge circuit is wired the same as BQ20Z75 EVM (HPA214).
I use SMBUS commands from a microcontroller to the BQ20Z75 to turn my load on and off, and the BQ20Z75 never enters "sealed mode."
The BQ20Z75 also turns off the charger - to - battery connection, (See SLUU277, Oct 2007, page 8, Q2 in schematic), and so the charger must withstand the battery being disconnected at any time (at charge termination) (by the BQ20Z75 EVM (HPA214)) while charging. When it does this, sometimes the BQ24765 fails (likely because of inductor dumping).
I have further tested this on the HPA349 EVM. Leaving the input adapter connected , leaving CE high, and connecting / disconnecting the battery. After a few tries, the BQ24765 no longer charges, and it is obvious that the power stage is destroyed, while the logic portions still function.
What would you recommend to prevent destroying the BQ24765 in my application?
It seems to me that the combining of HPA349 and HPA214 (or HPA059) as in SLUA533 is not a valid combination, in the sense that the BQ20Z75 can disconnect the battery from the charger, causing failure of the HPA349.
Mike