Hi:
I use TI TPS54308. I have some questions to consult, please help me solve them,thank you.
1.We put a magnetic bead on the DCDC output;The current magnetic bead is rated at 2.2A and can withstand 4.4A/20mS.I would like to ask you how long it takes to protect the output current of TPS54308 above 3A and cut off the output?
2.Chip PWM cycle refers to the chip internal switching frequency 0.35M, that is, 47uS?When the output is about 9V,47uS and the current is greater than 3A, can it be cut off?
3.In the specification, I(LIM_HS) max5.9A, I(LIM_LS) Max 5.5A, I want to know if it is larger than this parameter, can it be cut off?
4.In the specification, section 7.3.11.2, what exactly do 512 cycles and 16384 cycles refer to?Can you help to explain?
BR
Sunny