This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54201: 4x IR-LED with analog dimming on 12V

Part Number: TPS54201


Hello,

could you take a look at our schematic?

We want to use 4 pieaces of IR-LEDs with 100mA max current.

The PWM signal has 3.3V amplitude.

I was wondering whether we could use a smaller inductor.

BR

Michael